EIP.SYNCINFO
Description
EIP.SYNCINFO provides detailed information about the drive’s time sync object, which is required by the CIP Sync connection. This information aids in troubleshooting potential timing issues between the drive and controller.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-10-00-000 |
General Information
Variants Supported
EtherNet/IP drives: AKD2G-SPI
See Also
EIP.PLLMODE | CIP Sync Command Assembly Data Structure (105) | CIP Sync Response Assembly Data Structure (106)